Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Product List
Constant Current Regulators Slide 25

The yellow trace (TP1) shows the pulsating DC voltage from the bridge rectifier. The blue trace (TP2) shows that the peak voltage across the LEDs and resistor is controlled at 108 V regardless of input voltage. This is confirmed by the current probe (the green trace) measuring 25 mA in all cases. The blue trace also shows that the On-time for the LEDs will vary from 47% to 56% with a  +/- 10% change in the input voltage. This results in an approximate +/- 10% change in light output.

PTM Veröffentlicht am: