Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Product List
Constant Current Regulators Slide 20

In this diagram, Circuit A has a single CCR driving multiple strings of LEDs. This circuit is not recommended because it requires the LED forward voltages to be matched exactly which is not practical. Also if one of the LED strings fail, the remaining strings will carry the extra current and could be damaged. Circuit B has a CCR for each LED string which eliminates the need for LED matching and protects against string failure.

PTM Veröffentlicht am: