Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Product List
FlashCards-slide9

NAND Flash endurance can also be quantified in terms of the terabytes written (TBW) along with P/E cycles. The TBW of NAND Flash media, in simple terms, is influenced by the total capacity of the media, the endurance rating in P/E cycles and the Write Amplification Index/Factor. Write Amplification Index or Factor is the ratio of total bytes of data written to the NAND Flash media to the total bytes written by the host system.

PTM Veröffentlicht am: