Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Product List
FlashCards-slide10

There are general guidelines to follow to help maximize NAND endurance based on the end application. These guidelines can help the designer choose the best NAND architecture for the project: Ideally write files with size aligned to multiples of “Managed Block Size”. In embedded applications, log files for example are much smaller than the size of a Managed Block; in which case writing with file size aligned to multiples of “Managed Page Size” is recommended. Avoid writing very small size files and frequent update. Simplify disk partitioning structure. Avoid filling up the whole capacity of a partition and avoid filling up the whole capacity of the disk.

PTM Veröffentlicht am: