Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Product List
FlashCards-slide12

Data Retention is the ability of a NAND Flash cell to hold charge and thus store data. Over time, charge (electrons) may leak from the memory cells through the transistor floating gate resulting in a change in logical bit state and thereby potentially causing data corruption. Temperature variation significantly affects data retention as seen in this chart (MLC in this case). As shown here the higher the temperature, the lower the data retention. Also extreme cold temperatures affect data retention.

PTM Veröffentlicht am: