Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Product List
FlashCards-slide26

Different flash card form factors include varying levels of protection against power cycling. ATP microSD and SD cards are limited in real estate to include on board capacitors and hence employ ATP PowerProtector Lite which is firmware based power protection. ATP MLC Compact Flash also uses ATP PowerProtector Lite, however ATP SLC Compact Flash cards benefit from capacitance based protection – ATP PowerProtector in addition to the passive features from PowerProtector Lite.

PTM Veröffentlicht am: