Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Product List
FlashCards-slide8

Given a typical usable life requirement of 5 years, applications that write more than 1x-1.5x drive capacity per day will benefit from higher endurance memory such as SLC or aMLC. Write Amplification is significantly affected by data addressing and variable file sizes. Random addressed data with varying file sizes less than the NAND Flash page/block size is a worst-case scenario. Sequential addressing with files larger than the NAND Flash page/block size aids in minimizing Write Amplification by reducing the number of effective writes to the NAND Flash media.

PTM Veröffentlicht am: