Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Product List
FlashCards-slide7

Endurance requirements are heavily dependent on the type of client application data write patterns. Data logging applications typically operate with Byte/Kilobyte size files. Writing files to NAND Flash that are smaller than the inherent page/block size results in high Write Amplification which in turn greatly reduces usable life. This is owing to the internal program/erase algorithms used to write to NAND Flash and manage cell wear. The endurance requirement for a specific application should take into consideration expected usable life (in years), data write patterns/workload, NAND media endurance rating and total data written per unit time (DWPD – drive writes per day).

PTM Veröffentlicht am: