Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Product List
FlashCards-slide5

Internal processes within the NAND Flash memory device controller to manage the reading/writing of data and wear leveling increases the number of writes to the media beyond the number being transferred from the client. This increase in the number of writes is called Write Amplification, which in turn wears out memory cells. Write Amplification is measured in terms of a Write Amplification Index (WAI) or Write Amplification Factor (WAF) which are synonymous. Aligning NAND Flash write patterns to the underlying memory architecture can dramatically reduce wear on the memory device and increase its usable life.

PTM Veröffentlicht am: