Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Product List
SAM9 MPU Boot Solutions and Application Deployment Slide 8
The second case to consider is the boot from the embedded ROM. Our SAM9 MPU Boot ROM provides several applications such as:  - A 1st Level Bootloader called NVM Memory Bootloader that will call a 2nd one depending on the customer application. - An In-System Programming (ISP) Firmware Solution called SAM-BA Boot to program easily the external memories thanks to Microchip’s free ISP software called SAM-BA GUI.
PTM Veröffentlicht am: