Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Product List
SAM9 MPU Boot Solutions and Application Deployment Slide 16
We will now shift focus to standard application deployment. After power up, the code in Boot ROM is executed. An NVM memory bootloader may be used as a first level bootloader to copy in the internal SRAM a second level bootloader. In this example, the second level bootloader is the AT91 Bootstrap. This application is a bootstrap for SAM9 MPU microcontrollers. It can be uploaded and launched by the ROM Boot Program and can be used to configure the system and to download a larger application. Then, the 2nd level bootloader may (or may not) be used to download a 3rd bootloader such as the u-boot (Linux) or e-boot (Windows CE), which have many more features available for the OS development. Finally, the third level bootloader will call the final application: maybe Linux, WinCE or a stand alone application.
PTM Veröffentlicht am: