Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Product List
SAM9 MPU Boot Solutions and Application Deployment Slide 11
For SD Cards, there are two code requirements that must be followed: a boot.bin file must be written in the root directory of a FAT formatted SD card and the code size of this boot.bin must be at least smaller than the SAM9 MPU internal SRAM size. Once again, this is product dependent and must be checked in the Boot Program section of the product datasheet.
PTM Veröffentlicht am: