Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Product List
SAM9 MPU Boot Solutions and Application Deployment Slide 5
Reading out of a NOR Flash is similar to reading out of a random-access memory, provided the address and data bus are mapped correctly. Because of this, most microprocessors can use NOR Flash memory as execute-in-place memory, meaning that programs stored in NOR Flash can be executed directly without the need to copy them into RAM. That is not the case for NAND Flash memory in which programs cannot be executed directly; instead, code shadowing must be performed. Microchip’s boot ROM makes it possible to boot from one of these NAND Flash based memories which do not require an external NOR Flash.
PTM Veröffentlicht am: