Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Product List
SAM9 MPU Boot Solutions and Application Deployment Slide 2
A standard ARM9 MPU during a classical boot sequence will have to boot from a memory suitable for code execution such as NOR Flash. He will execute his main application out of that memory and will probably have to access a NAND for Read Only Data and an SDRAM for Read/Write Data and even Code execution. In such boot sequence, up to three external memories can be implicated and accessed by the ARM9 MPU.
PTM Veröffentlicht am: