Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Product List
SAM9 MPU Boot Solutions and Application Deployment Slide 7
The first case to consider is the boot from an external 16-bit NOR flash memory which is an eXecute In Place (XIP) memory. Different XIP memories can be used for booting purpose. At power up, the System Clock is the Slow Clock (32kHz) with the first instruction executed at the address 0x0. So at this step, no boot program has been executed so no device initializations have been performed. That means the user application running out of this memory must perform different initializations such as clock setups, timing configurations, and more.
PTM Veröffentlicht am: