Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Product List
SAM9 MPU Boot Solutions and Application Deployment Slide 20
Today, development tools integrate their own Flash loader utilities to program the application during debug phase which is the simplest way to debug an application. For the boards that do not embed any JTAG interfaces or for demo purposes, the SAM Boot Assistant (SAM-BA™) GUI is the solution. The SAM-BA software provides a means of easily programming various Microchip AT91 ARM Thumb based devices. It runs on Windows 2000 and XP and allows communication with the target device through an RS232 serial port, USB or a JTAG/ICE interface. The SAM-BA UI is based on a central DLL called AT91Boot_DLL.dll that can be used by the customer to create a custom GUI interface.
PTM Veröffentlicht am: