Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Product List
LED-Driver-Slide13
Here the initial calibration, as presented on the last slide, is compared with an additional technique called auto calibration. This technique runs a check at a given interval to see if there has been a shift in the characteristics of the system and is no longer operating on the edge of saturation. If this is the case, the power usage is no longer optimal and the power supply needs to be recalibrated. This is often the case in lighting systems that are turned on for long periods of time, causing temperatures to vary from 20 to 100° C. The auto calibration function can also be triggered on command.
PTM Veröffentlicht am: