Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Slide 49 Slide 50 Slide 51 Slide 52 Slide 53 Slide 54 Slide 55 Slide 56 Slide 57 Slide 58 Slide 59 Slide 60 Slide 61 Slide 62 Slide 63 Slide 64 Product List
Core-Microconverter-Slide42

For the bipolar transfer function, zero scale is represented by 0xF0000000 hex and full scale by 0x0FFE0000 hex. Note that the full scale result is not 0x0FFF0000 due to the fact that the differential result is +/-11 bits. When the ADC result is positive, the sign bit will be zero. For example, for a V+ input of 1.25V and a V- input of 1V the ADC will read the difference as 250mV. Assuming a reference value of 2.5V, the ADC will convert this value to 0x01980000 hex which converts to 249mV.

PTM Veröffentlicht am: