Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Slide 49 Slide 50 Slide 51 Slide 52 Slide 53 Slide 54 Slide 55 Slide 56 Slide 57 Slide 58 Slide 59 Slide 60 Slide 61 Slide 62 Slide 63 Slide 64 Product List
Core-Microconverter-Slide32

On this slide are some typical performance figures of the ARM7 core. The length of time to respond to an interrupt will vary depending on the current instruction being executed. The ARM7TDMI core contains a multiply instruction. For a 32 x 8 bit multiply, an instruction is executed in 2 cycles and for a 32 x 32 bit multiply, an instruction is executed in 5 clock cycles. One area the ARM7 processor is particularly good at is moving data. For example, a 1kB block of data can be copied from FLASH to SRAM in 1.1mS.

PTM Veröffentlicht am: