Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Slide 49 Slide 50 Slide 51 Slide 52 Slide 53 Slide 54 Slide 55 Slide 56 Slide 57 Slide 58 Slide 59 Slide 60 Slide 61 Slide 62 Slide 63 Slide 64 Product List
Core-Microconverter-Slide33

While the ARM7 processor is not designed for DSP tasks, many users might want to implement simple DSP functions. An un-optimized 4 TAP FIR filter would take 270uS while a 10 TAP FIR filter would take 1.7mS. The flash included on the ADuC702x is divided into 512 byte pages. The erase time for one page is 20mS with the write time being 20uS per byte. Once a page is erased, the bytes can be written individually without the need to write the whole 512 bytes at the same time.

PTM Veröffentlicht am: