Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Slide 49 Slide 50 Slide 51 Slide 52 Slide 53 Slide 54 Slide 55 Slide 56 Slide 57 Slide 58 Slide 59 Slide 60 Slide 61 Slide 62 Slide 63 Slide 64 Product List
Core-Microconverter-Slide24

Shown here is the ADuC702x series memory model. All interaction between the ARM7TMDI core and the peripherals on-chip takes place through memory mapped registers (MMRs) which are located at the top of the memory map. Memory mapped registers are the equivalent of the Special Function Registers or SFRs which users of the 8052 based parts would be familiar with. For example, an ADC conversion can be started by setting a bit in the ADC control MMRs with the ADC result being available in the ADC data MMRs once the conversion is complete. All other peripherals can be accessed in a similar manner.

PTM Veröffentlicht am: