Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Slide 49 Slide 50 Slide 51 Slide 52 Slide 53 Slide 54 Slide 55 Slide 56 Slide 57 Slide 58 Slide 59 Slide 60 Slide 61 Slide 62 Slide 63 Slide 64 Product List
ADuC7019 ADuC7020 ADuC7021 ADuC7022 ADuC7024 ADuC7025 ADuC7026 ADuC7027 ADuC7028

This block diagram shows a basic overview of the SAR ADC based ADuC702x family. Again, highlighted in blue is the analog section of the chip which include an integrated 12-bit SAR ADC with from 5 to 16 input channels (dependent on the specific model selected). The ADC inputs may be configured in Single-Ended mode, Fully Differential mode, or a Pseudo-Differential mode. However, in Pseudo Differential mode, an external bias signal is required. Also included in the analog portion of the diagram are up to four 12-bit DACs, a voltage reference, and an on-chip comparator.

PTM Veröffentlicht am: