Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Slide 49 Slide 50 Slide 51 Slide 52 Slide 53 Slide 54 Slide 55 Slide 56 Slide 57 Slide 58 Slide 59 Slide 60 Slide 61 Slide 62 Slide 63 Slide 64 Product List
ADuC816 ADuC824 ADuC834 ADuC836 ADuC845 ADuC847 ADuC848

Other peripherals in the analog area include two programmable excitation current sources and an internal reference. It is also possible to connect an external reference source – popular in ratiometric measurement applications like H-Bridge based designs such as pressure sensors and weigh scales for example. A single 12-bit DAC is also included in the analog portion of the device. The rest of the diagram shows the 8052 core, the RAM and FLASH Memory, communication interfaces (SPI, UART, I2C), timers, and a debug interface. The full list Sigma-Delta based devices is listed in the right hand column of the slide.

PTM Veröffentlicht am: