Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Slide 49 Slide 50 Slide 51 Slide 52 Slide 53 Slide 54 Slide 55 Slide 56 Slide 57 Slide 58 Slide 59 Slide 60 Slide 61 Slide 62 Slide 63 Slide 64 Product List
Core-Microconverter-Slide10

This table provides an overview of the 8-Bit ADuC8xx family of parts. The two left hand columns list the SAR-ADC based devices while the two right hand columns list the Sigma-Delta ADC based devices. There are 3 other which differentiate these parts from each other – 1) The ADuC81x/82x parts contained in the Row marked “Standard” contain a maximum of 8kB of Flash program memory, 2) The ADuC83x/84x parts in the large memory and Fast Core rows contain up to 64kB of Flash program memory, and 3) The ADuC84x parts in the row marked “Fast Cores” contain an enhanced 8052 core (Single Clock cycle per machine instruction).

PTM Veröffentlicht am: