Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Product List
High Speed LVDS Slide 9

As mentioned earlier, high-speed signals are distorted when sent thru cables and traces with the media acting as a low-pass filter attenuating the high frequency content. Equalizers compensate for this loss by boosting the high frequency portion of the signal. An ideal equalizer would have the exact opposite transfer function of the transmission media. Multiple Equalizer settings allow the device EQ to be closely matched to the media loss. Here we see the low, medium and high equalizer settings available with the DS25CP104.

PTM Veröffentlicht am: