Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Product List
High Speed LVDS Slide 26

In some cases it may be possible to control both sides of the transmission link – in which case EQ and PE can be used in conjunction. This example is using CAT 5e and a fail point of .5 UI (eye 50% closed on the horizontal axis). A combination of EQ and PE can achieve 30m at a data-rate in excess of 2 Gbps. Note the substantial increase in reach using signal conditioning. Various EQ and PE settings can achieve similar results – those listed exhibit the lowest jitter in this particular scenario. For example EQ MEDIUM/PE LOW is similar to EQ LOW/PE MEDIUM.

PTM Veröffentlicht am: