Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Product List
High Speed LVDS Slide 12

Media introduced ISI can be compensated using equalization at the receiver or, alternatively by using pre-emphasis at the driver. In the case of pre-emphasis, the rising and falling edges are boosted about the same amount as the expected media loss. As seen in the waveform, with pre-emphasis the signal leaving the driver is distorted, but if the setting is correct will end up with minimal distortion at the receiver. Multiple pre-emphasis settings are provided to allow a boost selection appropriate for the expected media loss.

PTM Veröffentlicht am: