Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Product List
High Speed LVDS Slide 14

Loss-of-Signal can be used to verify that signals are properly routed or cables connected prior to putting hardware on-line. In the case of the DS25CP104, an LOS circuit on each input monitors the signal strength and sets a flag in the event of no signal (or signal strength at ~25mV or less).

PTM Veröffentlicht am: