Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Product List
High Speed LVDS Slide 25

Evaluation boards are available for all of the new high-speed devices. As shown in this example, these boards all contain various embedded trace lengths to enable the user to investigate performance with different media without requiring external hardware. In this example there are 3 separate traces, 14, 28 and 42 inch traces embedded on the evaluation board.

PTM Veröffentlicht am: