Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Product List
HFE2500-Slide17

The HFE2500 part numbering system is simple to understand. The customer can select the output power, output voltage, and, if needed, the optional PMBus interface. The HFE rack nomenclature is very similar, this time there is a choice of input connectors, either IEC320 cables or screw terminal blocks.

PTM Veröffentlicht am: