Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Product List
PTC Overcurrent POSISTOR Slide 9
This shows the Operating Time in relation to ambient temperature. When the POSISTOR® is in a hot environment, it will start limiting current very quickly. For the above example, when 400 mA initially flows though a POSISTOR®, it will take less than one second to limit current to 200 mA.
PTM Veröffentlicht am: