Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Product List
PTC Overcurrent POSISTOR Slide 7
These charts show the Dynamic Characteristics of the POSISTOR®. Depending on the amount of current flowing through the POSISTOR and the ambient temperature, the time it takes the thermistor to react to an over-current event will vary. This time is called the attenuation time or operating time. Murata specifies “Operating Time” as the period of time that it takes the thermistor to decrease current from 50% of its initial value. Complete specifications for individual parts are given in our catalog.
PTM Veröffentlicht am: