Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Product List
PTC Overcurrent POSISTOR Slide 14
In motor protection circuits, a leaded POSISTOR® is well-suited for locked-rotor protection, and is easily installed in series with the motor. The resistance of a motor drops when its rotor becomes locked and current increases rapidly. In response to this increased current, the POSISTOR® increases its resistance quickly and limits the “over current” event. After the motor starts again, the POSISTOR® will automatically recover and return to its original resistance.
PTM Veröffentlicht am: