Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Product List
PTC Overcurrent POSISTOR Slide 10
Here is the line-up of the over current protection POSISTOR®. The 0805 or 0603 sized SMD type is available up to a hold current of 750 mA. The leaded type can handle a larger hold current than the SMD versions. A narrow tolerance type is also available for the 24 V to 140 V series in the leaded package. The “N” in the chart denotes the availability of narrow tolerance devices.
PTM Veröffentlicht am: