Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Product List
Tiva C TM4C123x FPU Slide 6

The floating point supports conversions between fixed-point and floating-point data formats, and floating-point constant instructions. It supports 32-bit instructions for single-precision data-processing operations, and has decoupled three-stage pipeline. There is hardware support for denormals and all IEEE rounding modes. The floating point unit also supports saturation math. In order to conserve power, the floating point can be disabled when it is not required.

PTM Veröffentlicht am: