Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Product List
Tiva C TM4C123x FPU Slide 16

The peripheral driver library in TivaWare™ for C Series includes a set of function calls, commonly known as APIs, which can be used to initialize and configure the Floating Point Unit without having extensive knowledge about various registers and bit configuration. More details about the functions, including the description, prototypes, and arguments can be found in the driver lib documentation, which is available in the docs directory of TivaWare for C Series. It is strongly encouraged that the user reviews these before starting to use these functions.

PTM Veröffentlicht am: