Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Product List
Tiva C TM4C123x FPU Slide 10

There are about thirty six instructions in the instruction set of the Floating Point Unit such as absolute value, addition, comparison, division, and multiplication of floating point operands. Note that the table shown on this slide does not include all the instructions. Refer to the ARM®Cortex™-M4 technical reference manual for the complete instruction set. Also note that in some documents floating point instructions may begin with letter ‘F’ instead of letter ‘V’; such instructions are equivalent. For example FADD.F32 is equivalent to VADD.F32.

PTM Veröffentlicht am: