Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Product List
Tiva C TM4C123x FPU Slide 2

Floating point is a method of representing real numbers on computers and is similar to the scientific notation of representing real numbers. Representing numbers using floating point provides a way to support a wider range of values as compared to fixed point representation using the same number of bits. Each number has an exponent and a fraction. There are several IEEE formats to represent floating point numbers such as half precision, single precision, double precision and quadruple precision.

PTM Veröffentlicht am: