Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Product List
ALD-Slide8

As previously mentioned, the output current can be reduced (and the LEDs dimmed) using either a resistor or an external voltage. If the analog dimming terminal is not used, it should be connected to ground with a 10 KΩ resistor to avoid overheating the device.

PTM Veröffentlicht am: