Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Product List
ALD-Slide7

Pin 4 of the device is the remote on/off input. To turn the outputs off, Pin 4 can either be pulled low or left floating. To enable the outputs, a voltage greater than 2.5V should be applied to Pin 4 typically by connecting it to the Vin terminal.

PTM Veröffentlicht am: