Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Product List
Special Func 2
In this example, the REF0CN register has additional bits that enable the new reference voltage features. For example, the REFBGS bit enables the 1x or 2x gain of the reference voltage. This provides a 1.2 V or 2.4 V reference to the ADC. This flexibility enables the designer to maximize the dynamic range of the system and increase sensitivity where necessary.
PTM Veröffentlicht am: