To start application development for the OTP devices, the code will first need to be developed on a flash-based device that can be re-flashed many times. This reduces development costs by not wasting OTP MCUs during the coding process. The kit provides a development daughter card called the C8051T62x EDB. This board has the C8051F34A flash MCU installed that has many of the same features of the OTP devices and can be used for the majority of the development as was seen from the last section. Install the emulation daughter board onto the mother board by connecting to the P1 and P2 sockets on the mother board.