Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Product List
Supply Volt 2

There are several considerations when choosing the specific device in the family. In particular, the number of pins in the package determines certain connectivity of the supply voltages. Some packages have a separate VIO supply pin that allows the connection of different logic levels to the MCU. In other cases, the package does not have a VIO pin external and the IO voltage should be treated as though it were connected to VDD. Another aspect to consider is the VPP voltage. If the system is going to take advantage of in-system programming, then a 4.7µF capacitor is required on the VPP pin. This is used to provide the programming voltage to the MCU and it is not recommended to attach any other components to this pin. If the system will not use the IAP feature, then the pin can be used as general purpose I/O.

PTM Veröffentlicht am: