Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Product List
cold chain
A globally emerging asset tracking application is cold-chain compliance. The FDA and other international agencies require all pharmaceutical goods, foods, and cosmetics to have their environment monitored during transportation. The US government also requires all logging dates to be stored electronically. The US cold-chain was established in the 1990s and has become the global standard. Recent requirements for data loggers include the ability to create a pdf file showing temperature and other environmental characteristics recorded by the data logger on-site, so that a file can be read out via USB immediately. The LAPIS microcontroller ML630Q466/Q464 have the capability to support all of these requirements with very few external components.
PTM Veröffentlicht am: