Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Product List
Detect-Slide17

The CL-DA and CL-DB detect switches can be used in communication devices or industrial equipment where presence detection of a device or detection of opening and closing are required. The CL-DA and CL-DB may also be used in A/V equipment to detect presence of media such as a DVD, or in OA equipment for paper-out detection. An example of opening and closing detection in a laptop computer is shown in the photograph on this slide.

PTM Veröffentlicht am: