Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Product List
Detect-Slide14

This is an example of how a detect switch works in the hot swap application. This example illustrates the function of the normally closed (NC) switch. When the handle is not in position, contact is ON. When the handle is depressed, it will push down the actuator of the detect switch and the contact will be turned to OFF. In the case of a normally open (NO) switch, the contact will be turned ON when the handle is depressed and the actuator is pressed down.

PTM Veröffentlicht am: