Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Product List
Connectivity in Control Systems Slide 7

Shown on this slide is the effect of loop delay, or output delay. Looking at a servo motor as an example, the larger the loop delay is, the longer the delay, or the slower the servo response becomes. As the loop delay increases, the ripple effect grows. There is a very small line right in the middle, which is the target that the application is to be as close to as possible.

PTM Veröffentlicht am: