Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Product List
Connectivity in Control Systems Slide 14

Shown on this slide are examples of some of the options for connectivity. These options include Ethernet and IEEE-1588, traditional USB, Control Area Network (CAN) , Field bus and Profibus which are derivatives of the CAN type standards, and RS232 and RS485. The Concerto™ devices are compatible with these standards. A newcomer is power line communication, ASTI, which is industry focused for metering and solar where direct endpoint to endpoint communication is not the primary concern. The Concerto devices do support multiple PLC communication protocols. These are all supported by the C28X control device.

PTM Veröffentlicht am: