Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Product List
Connectivity in Control Systems Slide 26

The final block diagram in this presentation is for an Advanced meter reading application, another rapidly growing space. TI has a complete advanced metering team. In this solution the Concerto device is running the PLC and working with an MSP430, the metering SOC. This combination can do the AC/DC conversion, the system conversion, and then it can drive either out to a home network or wireless LAN or WAN with external devices. There are a variety of different applications that can be done with this device, these examples only touch the tip of the iceberg.

PTM Veröffentlicht am: