Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Product List
Connectivity in Control Systems Slide 20

This slide shows the different types of PLC technologies, standards, and regulations. These are S-FSK, slow, 2.4 kilobits per second, single carrier. There are thirty six carriers in the PLC OFDM, which operates at up to 35 Kbps, and the carriers can be multiplexed on that. PLC OFDM is IPv6 compliant. There is also a ninety seven carrier version of OFDM which is 128 Kbps compliant and is backward compliant with the IPv4. TI supports Prime, G3, and the IEC 61334 standards. Additionally, the CENELEC, FCC, and ARIB different regulations for worldwide standards are supported.

PTM Veröffentlicht am: